מחירי המוצרים באתר
בעקבות עבודות שדרוג האתר - יתכן וחלק מהמחירים לא מעודכנים



The world’s first steam-powered, interurban railway transporting both passengers and goods opened up almost 200 years ago, linking Manchester and Liverpool in the UK. In the years since, the rail industry has seen tons of new innovations of rail technology which has led to it being what it is today, such as automatic signalling, electrified railways, automatic half barriers and warning systems. Nowadays, trains are one of the most common transport options available and are usually the most suitable means to travel between cities. In 2020, passengers travelled around 378 billion km on European railways.
So, why does the railway industry need to innovate?
Despite its popularity, the railway industry is still not perfect and can be improved in a variety of ways. One of the main priorities for engineers and designers in the rail industry is speed, which can always be improved upon when better technology is developed. This is especially important when passenger demand for trains is high, as they can be more effective at transporting a larger number of people. Faster trains can also directly compete with air travel, meaning lower emission levels.
The EU has a mission to be carbon-neutral by 2050, and the railway industry has a part to play in helping the EU achieve this goal. Some technologies support the use of electrified railways, which would significantly lower emissions produced by conventional trains. Another aspect which is improved with better technology is safety, as the risk of human error can be replaced by adopting automatic processes instead. Over the years, we’ve seen lots of innovations which have aimed to tackle these issues, some have been successful and some haven’t. Take a look below at the 6 best rail technology innovations right now.
Train Innovations
High-speed rail is the fastest way to travel between major cities. Some high-speed trains such as the Shinkansen (bullet train) in Japan and TGV in France are capable of reaching speeds of up to 320 kilometres per hour. It meets the increasing demand for faster and better travel from A to B and around urban areas, reducing congestion and improving mobility. At such speeds, these kinds of trains offer a competitor to air travel, whilst being around eight times more energy-efficient, according to the International Association of Railways (UIC).
High-speed trains are only currently in operation in 16 countries around the globe. Most countries have dedicated tracks and routes for high-speed rail, however they can also operate on conventional tracks at reduced speeds. Roof-mounted pantographs and overhead supply lines generate the power to drive the trains, which often have two synchronised engines at either side.
Maglev, short for magnetic levitation, refers to trains which levitate around 10 cm above the ground. Unlike traditional rail technology, maglev trains don’t have wheels and instead use electromagnetic forces to lift the train above the tracks. The magnets used for maglev trains are superconducting, meaning that when they’re cooled to -450℉, they’re able to generate magnetic fields ten times stronger than regular electromagnets, which allows them to lift and drive the train forward. This means that there isn’t any friction involved with these types of trains, allowing it to travel at incredible speeds. In fact, the fastest a maglev train has travelled is 603 km/h.
But it’s not just the high speeds which makes maglev trains so appealing. The use of electronic propulsions systems reduces the use of fossil fuels for power and limits emissions. With the absence of friction on the tracks, maglev trains generally require less energy to maintain speed, and the regenerative braking system reuses energy that would be lost in conventional trains. Without the need for contact, it also means that less maintenance work needs to be carried out on the guideway and trains as the risk of wear and tear of components is significantly decreased.
The concept of Hyperloop technology was first introduced back in the 18th century by British inventor George Medhurst. Since then engineers and researchers have been exploring similar concepts for years, and it was later picked up by billionaire Elon Musk in 2013, with his own take on the idea for his Hyperloop Alpha project. In 2021, the global hyperloop market was worth 1.2 billion US dollars and is expected to reach 6.6 billion US dollars by 2026, at a compound annual growth rate of 40.4% in those five years. However, we are still at least 7-8 years away from hyperloop rail technology being ready.
Hyperloop enables high-speed transportation by using low-pressure tubes to transport pods. The pods travel through vacuums which almost eliminates air resistance, allowing for incredibly high speeds of up to 1,100 km/h. The pods will be transported using magnetic levitation technology, meaning that although passengers will be travelling at rapid speed, they should still be able to enjoy a comfortable and quiet journey. In addition to this, with fully-electric and energy-efficient operations, Hyperloop is a sustainable form of transport, and one that could be key in Europe’s plans to become climate neutral by 2050.
At the moment, lots of companies are actively testing and developing Hyperloop technology. However we are still at least 7-8 years away from hyperloop rail technology being ready. Europe’s only Hyperloop test location is in Munich, Germany, called the TUM Hyperloop. It feels like a long time before we will see this futuristic-looking technology in action, but when it does start transporting passengers, it might become the new norm.
Other rail technology innovations:
ATO systems refer to the technology which allows trains to operate with little to no human intervention. The systems use a combination of sensors, computers and communication platforms to control the speed, acceleration and braking of trains. ATOs contribute to a safer railway network by minimising the risk for human error, as with precise control of train speed they can maintain safe distances from other trains and prevent collisions. They’re also more energy-efficient as they can optimise energy consumption and reduce waste, whilst also having the potential to incorporate regenerative braking systems.
Augmented reality (AR) and Virtual Reality (VR) can be adopted to offer immersive and effective training solutions for rail staff. The result is a realistic environment which gives drivers, conductors and maintenance workers experience of a real-life situation which can be done in their own time. AR and VR can also be used in the design and planning of new networks, tracks and infrastructure, or any modifications to existing networks as rail engineers and planners can use them to better visualise and evaluate proposed designs. By leveraging digital models to showcase ideas, it gives stakeholders or investors a better picture of what the end product will look like.
PTC is an advanced safety system that works on the principles of automation. By monitoring trains in real-time using GPS technology, PTC systems are designed to improve safety by automatically intervening if any unsafe conditions that could lead to collisions are detected or predicted. With all information collected at a centralised control centre, the PTC systems can monitor and control train speeds based on a variety of factors such as conditions, track curves, gradients and more. If a train exceeds the speed, the system can automatically apply the brakes or signal audible or visual warnings to the driver.